HI TI,
There is currently a project that will require two-rail power monitoring. Is there a recommended IC?
Can the address of smbus be set by myself?
Br,
Delun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Delun,
We have many options that you can narrow down here. The first question is do you need a Dual channel. Unfortunate we only have singles and a three channel device.
3channel- INA3221.
If you are looking for single we just started sampling the INA228 with 20 bit resolution. Or lower cost INA237 with 16 bits or resolution.
About the I2C address each device will have limited addresses you can use and normally controlled through address pins.
Hello Delun,
The schematic looks fine just be aware that all the pull-ups resistors are in parallel. If you add more I2C pins you will have a much larger load if you include a pull up resistor for each device.
Hi Javier,
If the pull up resistance is changed from 10k to 4.7k, will it be better than now?
BR,
Delun
Delun,
You can keep it at 10k. I was just mentioning if you have other pull up resistors(not on this schematic page) you may need to be aware they are all in parallel and can decrease your overall pull up resistance.