Hi team,
My customer would like to see the efficiency at 3.3Vin and about 0.6V/20A output. Could you provide the data?It is wished to be beyond 85%.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer would like to see the efficiency at 3.3Vin and about 0.6V/20A output. Could you provide the data?It is wished to be beyond 85%.
Thanks.
Hi Jerry,
Let me check and get back to you.
Regards,
Gerold
Hi Jerry,
At the moment we dont have efficiency data with 3.3V Vin.
regards,
Gerold
We do not have VIN = 3.3V data, or 0.6V output data, but I can make some estimations based on the data we do have.
The datasheet shows a VIN = 5V to VOUT 0.8V @ 20A with 90% efficiency. That represents 1.77W of loss (16W / 0.9 - 16W). Holding that same loss for 3.3V to 0.6V output will give an efficiency of 87%.
Please note - the TPS546D24A will require a >4V bias voltage for VDD5 or AVIN to power the MOSEFT drivers at 3.3V input. If no 5V bias voltage is available, and the customer does not want to use a charge-pump to make a 5V supply, there is a discrete voltage doubler circuit that can use the SYNC output pin of the TPS546D24A to boost a 3.3V supply voltage to power AVIN above 5V and use the internal VDD5 LDO to regulate the gate drive to 4.7V.