This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561EVM-011: Voltage dropped issue found on BQ27z561EVM-011.

Part Number: BQ27Z561EVM-011
Other Parts Discussed in Thread: BQSTUDIO

Hi,

I am using BQ27Z561EVM-011, 1s6p battery cell, and 1.5A load.

1. I have triggered the learning cycle. At the stage of discharge, when I connect 1.5A load to BQ27z561EVM-011, my battery pack directly dropped 0.4V voltage.(3.37 V dropped to 2.98 V) So I can't able to complete the learning cycle. What is the reason behind that? I can negate +/- 25mV dropped but here more than 100 mv. When I have connected load directly to the battery it will dropped only 10mA. Is there any configuration needed in BQStudio?

2. Also, I have noticed that when I connect the battery pack to the BQ27z561EVM-011 kit and got 3638 mV voltage on BqStudio instead of 3370 mV (actual battery pack voltage). What is the reason behind that? I wasn't able to understand this behaviour. 

Please help me.