Hi team,
the customer is trying to solve for transformer DMAG(Min) from equation 10 in the datasheet. they are getting ~14us because the input voltage is so high and the NPS can't go higher since they still want to support lower input voltages (110-480VIN).
Is the target supposed to be 1.1us or is that just the absolute minimum you can have and 14us is ok?
additionally, in SLUC408B (excel design tool), line 113 shows 600V as the max drain voltage of the FET. my customer wants to use 1000V rated FET but the line is not a user-input cell. is this a bug?
Finally, apart from the SLUC408B and the datasheet, is there any other documentation we can provide to help with transformer design?
Thanks,
Kevin