This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561EVM-011: Update status never updated to 06.

Part Number: BQ27Z561EVM-011
Other Parts Discussed in Thread: BQSTUDIO

I have triggered the learning cycle with the following parameters.

I have used the INR18650A battery as a 1s6p pack. I have 1.5A load and 4.0 V charger.

1. Start the learning cycle with the discharged battery (3.3 V). The update status is 0x04. 

2. Wait for the fully charged (4.0V). Relax till VOK should clear and REST is set. QMAX is toggled and update status is 0x05 now.

3. Start the discharge cycle with 1.5A load. Wait for to discharge till 3.3 V. Relax for 5 hr. But update status is not updated to 0x06. What is the reason behind this? 

I have attached config.gg file and log files. Please help me.

Advanced Charge Algorithm Low Temp Charging Voltage 4000 mV
Advanced Charge Algorithm Standard Temp Charging Voltage 4000 mV
Advanced Charge Algorithm High Temp Charging Voltage 4000 mV
Advanced Charge Algorithm Rec Temp Charging Voltage 4000 mV
Advanced Charge Algorithm Termination Config Charge Term Taper Current 300 mA
Gas Gauging Current Thresholds Dsg Current Threshold 60 mA
Gas Gauging Current Thresholds Chg Current Threshold 75 mA
Gas Gauging Current Thresholds Quit Current 40 mA
Gas Gauging Design Design Capacity mAh 15000 mAh
Gas Gauging Design Design Capacity cWh 5400 cWh
Gas Gauging Design Design Voltage 3600 mV
Gas Gauging FC Set Voltage Threshold 4000 mV
Gas Gauging FC Clear Voltage Threshold 3900 mV
Gas Gauging TC Set Voltage Threshold 4000 mV
Gas Gauging TC Clear Voltage Threshold 3900 mV
Gas Gauging State Qmax Cell 1 2500 mAh
Gas Gauging State Cell 1 Chg Voltage at EoC 3990 mV
Gas Gauging State Current at EoC 300 mA

Gas Gauging IT Cfg Term Voltage 3300 mV

1407.gg.csv

1407.log