Part Number: LM74700-Q1
Hi team,
I have a question about MOSFET selection for LM74700-Q1
Customer would not like to use low RDS(on) MOSFET. (because of the cost)
Datasheet said reccomended RDS is between 22mV/Id and 100mV/Id.
ID that they will use is 2A and RDS that they want to use is 60mΩ ~ 80mΩ.
Are there any problem or bad effect of higher RDS on?(for example longer on/off transient time)
and also on datasheet, gate Vth recomended 2-V to 2.5-V maximum.
if Vth exceed this value, what is the bad effect?
best regards,
Takuya