Part Number: CSD95490Q5MC
Other Parts Discussed in Thread: TMS320F28379S,
Tool/software: Code Composer Studio
I want to using TMS320F28379s to control CSD95490Q5MC.
But, I find that the EN/FCCM pin on CSD95490Q5MC has a internal pull-down resistor.
I configured the PGPIO13 pin, which is direct connected to EN/FCCM(pin 11), as input or open-drain output, but it can't ENABLE diode emulation mode(DEM) for sync FET.
And the measured level on EN/FCCM(pin 11) is low.
code:
1. Configure the PGPIO13 pin as input
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO13 = 0; //
GpioCtrlRegs.GPAPUD.bit.GPIO13 = 1; // Disable pull-up on GPIO13
EDIS;
2. Configure the PGPIO13 pin as open-drain output
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO13 = 1; //
GpioCtrlRegs.GPAPUD.bit.GPIO13 = 1; // Disable pull-up on GPIO13 (EPWM7A)
GpioCtrlRegs.GPAODR.bit.GPIO13 = 1;
EDIS;
GpioDataRegs.GPADAT.bit.GPIO13 = 1;
How can I configure the PGPIO13 pin to ENABLE diode emulation mode(DEM) for sync FET?
Thanks