Hi
Could you help check the TPS55288 schematic as below and any need to adjust?
Thank you so much
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you help check the TPS55288 schematic as below and any need to adjust?
Thank you so much
Dear Sir,
It seems you want to use TPS552882 non-I2C version. Right?
I found the output power is very big, 5V/12A and 3.3V/12A, which is pretty big totally. So the output power will be around 100W, right? This is already near the maximum limit of TPS55288, to handle the thermal, you need to use at least 6-Layer board to handle it.
I will check the schematic in detailed after get your reply.
Hi Helen
Thank you for your reply
When is the TPS552882 product release schedule? P2P TPS55288 ?
Dear Sir,
Yes,TPS552882 is pin to pin with TPS55288. It will be RTM released at the end of this year. But we already have samples now.