Other Parts Discussed in Thread: LM46002, LM5164-Q1, LM5164
I've used Webench for the following design:
24V In
-17V Out @ 0.5A
500kHz switching frequency
The Webench design did not include the snubber R/C that datasheet and eval board shows. Would these still be a good idea for this design? Would I connect them to GND or somewhere else?
I'm presuming I need to connect the EPad to the Output rail? That's not going to be great for sinking heat out of the device.
This part needs a lot of external components. Is there another part that requires less?
Thanks,
G