Hi,
From 9.2.2.4 of the datasheet
"The maximum inductance is limited by the minimum current ripple required for the current mode control to perform correctly. As a rule-of-thumb, the minimum inductor ripple current must be no less than about 10% of the device maximum rated current under nominal conditions."
I'm trying to calculate the Lmax value with equation 4 (page 22) so I will need to know the device maximum rated current.
Can you confirm that Equation 1 on page 16 should be used to determine the device maximum rated current?
Should I use the typical or max value for ILIMIT and ISC in equation 1 to determine the Lmax?
-Kelvin