Hi Experts,
I am using UCC21520 to drive led lamps ,So the issue is that the output side of the IC is getting shorted by a surge of as little as 1.5V above our 24V supply(Total of 25.5V for the IC which is it's upper cap). So could you please suggest if any circuit changes required to avoid spike, surge during switching and also if higher rating IC is available with similar channel support. The surge is mainly happening while connecting supply wires, when there is a little spark produced at the contact.