This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULN2803A: i need information mentioned below

Part Number: ULN2803A

Hi, i need to know few information listed below for the part ULN2803A .

1. Current status of the part.

2. If active, then how long it will be supported.

3. Is there any EOl or PCN issued.

4. RoHS and Reach document proof needed.

Kindly respond me as soon as possible.

Thankyou

  • Hi,

    Welcome to E2E!

    As of right now the ULN2803A is in production and will continue being supported as long as the device remains in production. It is very hard for a device to EOL so the production of the ULN2803A stopping should not be concern.

    There a no EOL or PCN's in progress for this device

    For the RoHS and Reach document proof needed would you be able to share an example of the type of document you're looking for?

    • In the datasheet of the ULN2803A in the Package Option Addendum" section(Pg. 14) we include in the table that the device is RoHS compliant
    • On TI.com you can also find a downloadable spreadsheet (Link) for the ULN2803A that state that the ULN2903A is RoHS and REACH compliant

    Best regards,

    Andy Robles