The TPS7H3301HKR datasheet says VTTREF buffered reference = ±15-mV accuracy. But the JEDEC standard says VTTREF has a required range of 0.49 * VDD to 0.51 * VDD. For a VDD input voltage of 1.35V - which the datasheet says is allowed - the JEDEC limits are 0.6615V to 0.6885V, or 1.35V/2 ±13.5-mV. So the JEDEC specification is tighter than the device specification.
Is there something I am missing here? Is there an argument as to why the IC is acceptable in this application?