Hi E2E,
Good day!
We just need some clarification regarding the minimum required input voltage for this part. On page 3, note 2 states that Vin mimum is equal to Vo + Vdo. Vdo values are indicated on page 5. However, on page 4, Note 4 states that the Vin minimum is either 2.7V or Vo + 1V, whichever is higher. Also, note 5 states that if Vo is less than or equal to 1.8V then Vin minimum is 2.7V. Else, if Vo is greater than or equal to 2.5V then Vin minimum is Vo + 1V.
Kindly explain these conditions.Thank you.
Best regards,
Franz