[OCVFR]: An OCV reading is taken when a dV/dt condition is met. This is not the case if charging stops within the flat voltage region.
By default, this flag is set. The device will take a 48-hour wait before taking an OCV reading if charging stops below the FlatVoltMax. A discharge will not cancel this 48-hour wait. The 48-hour wait will only clear if charging stops above the FlatVoltMax level. Setting this flag to 0 removes the 48-hour wait requirement, and OCV is taken when the dV/dt condition is met. Removing the 48-hour requirement can be useful sometimes to reduce test time during evaluation.
May I know the range of flat voltage region of LiFePO4? Can I set OCVFR flag to 0 in normal release code? what's the impact?