This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116: TLC59116 LED driver

Part Number: TLC59116

i am developing LED module by using TLC59116

i designed circuit 

and i connect it to RGB LED (https://lcsc.com/product-detail/Light-Emitting-Diodes-LED_61-238-RSGBB7C-B02-ET_C130391.html)

among 16 channels, some of LED is bright, but some is not

like below left one is good, (output channel 0~7, and 13) rest of them is not good 

i measure the voltages

input volatages are different

output 0-7, 13

5V -> (LED) 1.45V

output rest of them

5V -> (LED)  1.40V 

am i missing somthing?