Hi,
I'm currently using the LMR16006 for one of my products. I'm interested in using it for another project, but a question was raised about the spectrum of the output voltage. I'm using the buck converter to power a sensor that is very sensitive to 10-25kHz power supply noise. I noticed that the switching frequency range of the LMR16006 is at least 10x higher than the bandwidth that I'm concerned about. Should I be concerned about sub-harmonics of the switching frequency creating 10-25kHz spurs on the output voltage? Is there any information that I can find about what the output spectrum might look like. For reference, I'm looking to convert from +9 to +18V input down to +5V output.
Thanks for the help!