This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM23600: lmzm23600

Part Number: LMZM23600

Hi 

i'm designing a 5V to -4V converter.

i'm running the pspice adjustable model - downloaded from TI. 

feedback resistors are 75k (FB to VOUT) and 25k (FB to VOUT_IBB)

when running simulation voltage is -12V and then climbing to -4V. 

that is a problem because FB to GND start from 8V (Absolute max rating is 5V)

Please assist

Thanks

OR