Dear All,
Am working on Figure 7.3 of Bq76940 datasheet for Charge Path Fall Time & Rise Time @ Gate to Source pins of Mosfet.
Am obtaining 2.5msec fall time @ Gate to Source Pin of Mosfet over oscilloscope..Below is the circuitry i have used.
I wanted to understand the significance of reducing R2 @ Charge Path circuitry.
I Mounted following :-
- R1-1 mega Ohm Fall TIme Obtained is 2.5 mili second.
- R1-100K Ohm Fall TIme Obtained is 1.25 mili second.
- R1-10K Ohm Fall TIme Obtained is 500 micro second.
- R- 1K Ohm Fall TIme Obtained is 50 micro second.
And on the Discharge path with 1Mega Pull Down, Both Rise & Fall time are same approx 2.5 micro seconds.
Above readings which, i have observed with MCP1416t-ET Driver instead of AFE CHG & DSG Driver pins(Because when I Use AFE Driver Pins, I get following )
- Discharge path Rise Time – 300 micro seconds
- Discharge path Fall Time – 120 micro seconds
- Charge path Rise Time – 300 micro seconds
- Charge path Fall Time – 4 milli seconds
, means i have Bypassed CHG & DSG pins of AFE to trigger Mosfets, and instead of it i have used MCP1416t-ET Driver to Drive Mosfets.
Also i have placed single Mosfet only in parallel and 2 mosfets in series with Common Drain Configuration .
So please help me to understand, why if i use Gate-Source Pull Down of 1 M Ohm, than Fall time are not equal , for both (Charge & Discharge paths)(Discharge Path 2.5micro sec Fall time & Charge Path 2.5 milli second Fall time @ Respective Gate-Source Pins of a Mosfet?)
Also help me to understand scenario , when Pack- will be lower than Bat- or VSS or Ground? Am unable to visualize it.
Also share use of Keeping R1,R2 at CHG path @1M Ohm . Can it be increased?
Rohit