Other Parts Discussed in Thread: BQ24780, BQ24800,
Hi,
BQ24780 can detect AC charger input by ACDET > 2.4V and it can operate under 26V. The high operating voltage range is way higher than our system application.
So I would like to add ADC input to read AC charger input level and let SW control ACFET & RBFET manually when AC charger input is higher than 18V (e.g.). Then valid input range should be between 2.54V on ACDET and 26V at VCC.
However, I can't find a way to control ACDRV to pull to low manually or by SW.
How can I put the signal to low when we want?
Regards,
Han