Hi TI support,
Good day. I have 3 question need advice. The chipset that I use is TPS3808G01DBVRG4
1) Can I connect the SENSE to a voltage source that higher then VDD? Below are my application:
MR = Not connected, CT = not connected, RESET = pull-up to 10Kohm, VDD = 2.8V, SENSE voltage range= 0V - 5V
2) I found that when I connect to a 6KHz square wave (high level = 4.5V; low level = 1.0V). Although VSENSE > VIT, I still get some unexpected LOW RESET (asserted 20ms, please refer to diagram below). My SENSE doesn't connect any capacitance. What could be causing the problem? Is that related to transient?
Note: The unexpected LOW RESET doesn't occur when there is a 1nF caps at SENSE.
3) Any dv/dt requirement for SENSE? Any abnormality will occur if I connect SENSE to a switching source eg: 10KHz?