Hi team,
My customer is using the TPS2553 now, the schematic is below, When the load side has a inrush current during startup period. The peak current will be 2.8A about 150us from the waveform. As you can see the device may trigger OCP, but the Vo start to drop more than 1v when the inrush current disappear. i have let the the customer remove the L53 and use the cable to do the test, the same phenomenon. Do you have some ideas about the weird phenomenon?( in my opinion, the device will not have such large voltage droop with no current limit after the inrush current). Thanks.
(the blue is the output cap voltage, the purple is the inductor current)