Hello.
We use the LP2980AIM5-5.0/NOPB on our boards to genearte 5 V from 12 V, to power a digital circuit which draws about 3.5 mA.
During recent tests in the climatic chamber, we noticed a wrong behaviour of this regulator.
When the temperature of the IC (measured on its plastic body) reaches 99 °C, the output voltage starts to increase and is out of specifications.
I provide our measurements below.
T(IC) [°C] | Output voltage [V] | Notes |
<99 | 5.014 | |
99 | 5.180 | after 1 minute |
99 | 5.614 | after 1 additional minute |
100 | 5.870 | after 1 additional minute |
100 | 6.150 | rises quickly |
<99 | 5.014 | in about 18 seconds |
Then this cycle repeats again and again, affecting the function of our boards.
Other info: at the output of the regulator we have a 10 uF, X7R capacitor.
Q1. What could be the reason of this behaviour?
Q2. In the datasheet of this regulator it is stated that there is a thermal shutdown, but we expect that in this case the output voltage would drop to 0 V. So, what we observed is not related to thermal shutdown of the IC, is this correct?
Thank you.