This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
This is a rather older, non-synchronous device, and as such it does
not have a "light-load" mode. Most of our newer devices will reduce the
switching frequency with light or no-load; to lower the input current and improve the efficiency.
Please look at the LMR33630 family of devices.
They are offered in the same package and will have
a no-load input current of about 25uA (see data sheet).
Also, see application note SLYY189.
Thanks
Hello
The best way to tell is to look at the data sheet. If it does not state a light load mode or the input current at light load,
then you can expect it will be somewhat high. The non-switching Iq is not a good indication. Please see SLYY189 for
details.
Thanks
Thanks for your application note. Now i have a better understanding while reading datasheets.
Also, replaced TPS54308 which TPS54302 which has 70% efficiency at light load conditions or 1mA as per datasheet.
Results: 12V in, 5V out, No load
Input Current is 0.08mA
Results: 12V in, 5V out, 10mA output load.
Input Current is 4.7mA