Other Parts Discussed in Thread: CSD19534Q5A, TPS2819,
I am getting a non-monotonic rise on my gate signal causing very high switching losses which is resulting in damaging my FET, I have tried multiple different FETS ranging from (Qg of 55nC, RDs(on) of 2.8mΩ) to (Qg of 6.9nC and RDs(on) of 32mΩ) and in-between, I experience this issue with all of them.
Power level do effect the edge although the glitch is still present at very low power levels.
The circuit is a 24V to 48V 60W boost converter running at 700Khz
Thanks