Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100
Hi
At -35degC, I am seeing non-linear SoC jumps
At -35CdegC, BQ34Z100-G1 jumps down from 95% to 0% SoC when my system draws 2A from frozen LFP battery and battery voltage temporarily drops to 10.8V for 300ms. I understand that is related to SoC 0% threshold voltage.
Immediately after 2A load removal my battery voltage recovers to 13.1V-13.4V. To recover for this temporary anomaly my system issues RESET x41 command. Only 20% of time FuelGauge reports non-zero SoC.
Through experimentation I found below.
Vbatt 11-13.29 = SoC 0%
Vbatt 13.3 = 51%
Vbatt 13.4 = 62%
Vbatt 13.8 = 100%
What parameter can I change so that I can get non-zero SoC above 11V after RESET x41 command?
Regards,
Padam