Please find the attached circuit diagram, we are facing issues with BQ25713.
We are giving input 12V DC, we are getting Q1 output as 1.6V DC,as we were expecting 12V DC
The voltage at H1DRV1 is also 1.6V (gate of Q1).
While measuring REGN it was showing 8V DC.
VBUS is 12V DC.
As the recommended voltage at REGN is 6V,what will be causing it to 8V level ?
Help us resolve this problem ( For getting 12V DC Output at VSYS).