Hey folks,
I have a question regarding the TPS2561ADRC RILM.
The datasheet states:
The overcurrent threshold is user programmable via an external resistor, RILIM. RILIM sets the current-limit
threshold for both channels
Question:
Is the IOS limit set by the RILIM resistor the current limit for each channel or the current limit for both channels. In other words if I set the current limit to 900 mA, can both outputs supply 900 mA simultaneously or does this mean that the sum of the output currents (IOUT1 + IOUT 2 will be limited to 900 mA?
Thanks,
AH