Hello Team,
do we have the values for the voltage limits of the gate-to-anode (min/max)?
LM74700 will be used in 'regulated conduction mode'
Many Thanks
Josef
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
do we have the values for the voltage limits of the gate-to-anode (min/max)?
LM74700 will be used in 'regulated conduction mode'
Many Thanks
Josef
Hello Josef,
Gate-source voltage maximum is 14V.
However, minimum voltage is dependant on the load current, MOSFET used.
Could you please share the MOSFET part number and the minimum load current and maximum load current.
Regards,
Kari.
Hello Kari,
The transistor used is BUK7Y2R5-40H from Nxperia, regarding the Load current, the max value is 21.58A, and the min value is 9.69 during normal operation and 625 mA during standby mode.
Thank you in advance.
Best regards,
Youness
Hello Youness,
Attached document discusses gate voltage in ideal diode controllers in detail along with an example of a MOSFET DMT6007LFG.
Ideal_Diode_Controllers_Gate_Control.pdf
Let us know if you have more questions.
Regards,
Kari.