This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS709-Q1: Can the TPS709 Q1 supports Automotive Load dump ( 34V)

Part Number: TPS709-Q1
Other Parts Discussed in Thread: TPS709

As per GMW 3097 for General Motors. it requires the load dump @ 34V Ri 2 ohm 10 pulses 15 seconds apart.

We have 33.7V @400ms applied to the IN pin. The data sheet calls out a max of 32V.

Does the part can handle the 34V load dump?

Edgar