This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1117LV: output accuracy under

Part Number: TLV1117LV

Hi,

customer love the 1.5% accuracy  of TLV1117LV. but asked below 2 question:

Q1: if TLV117LV can keep this accuracy within the all temperature Range :–40°C to +125°C. 

Q2: could you please comment if this device can work in a high humidity environment such as 90%。 how humidity impact the perfomance of this device?

looking forward to your feedback. thanks. 

  • Hi Yuan,

    Q1: if TLV117LV can keep this accuracy within the all temperature Range :–40°C to +125°C. *When you see a minimum and maximum value in our electrical characteristics table. This is over the full temperature range (-40 to 125C):

     

    Our TLV757 was designed as a next-gen version of this device. This has much tighter accuracy:


     

    Q2: could you please comment if this device can work in a high humidity environment such as 90%。 how humidity impact the perfomance of this device?* The Device is rated as MSL-1 so for storage, its moisture sensitivity has an unlimited shelf life. I think the biggest concern is the potential for condensation and leakages pin to pin.

     

    Does this help to clarify?