This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV703: TLV70318 startup waveform

Part Number: TLV703

Hi team,

My customer is using the TLV70318 now. Input 3v3, output 1v8. As you can see, the Output startup waveform slew rate has two period has two slew rate. It seems the device trigger OCP or OTP during the startup period. Or OCP threshold is different during different startup period. i have let them share the details to see the current. Do you have some experience about the phenomenon? Thanks.

yellow is the input voltage, purple is output voltage, blue is EN.

stage 1: 0v->1.2v, 8ms, stage 2 1.2v->1.8v 40us

i have used the ic=cdu/at to get the 3mA during stage1, 300mA during stage 2.

Thanks.