Other Parts Discussed in Thread: TLV767
Hello E2E,
We could see the overshoot issue during startup on TLV1117-18 converting 5Vin to 1.8Vout.
Is it normal?
if not, how to solve the issue?
BR,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jason,
Are those ceramic capacitors at the output? The TLV1117 needs an effective ESR between 0.2 and 10 Ohms:
if these are ceramic capacitors, adding series resistance to meet the ESR requirements could help to reduce this overshoot. Note a modern update to the 1117 is the TLV767.
I hope this helps.
John,
We try to remove the original ceramic cap and add a 4.7uF Electrolytic capacitor, but the overshoot issue.
we just want to know if it is normal behavior on TLV1117-18?
in addition, is TLV767 p2p with TLV1117-18? If yes, could TLV767 fix overshoot issue at startup?
BR,
Jason
Hi Jason,
I believe the overshoot issue you are seeing is simply due to the lack of inrush control. Unfortunately, the TLV1117 is a very simple regulator.
As for the TLV767 unfortunately it is not P2P with the TLV1117 as in addition to superior inrush control it has an enable pin and a remote sense for fixed versions. This helps to improve regulation accuracy over load.
I hope this helps.