Hi TI expert,
Currently I'm designing a boost topology, I see the LM5122 is a good controller that can be used in normal condition, the feature and performance are very good. But the VIN max of LM5122 is only 75V, is there any related device that VIN could support at least 90V?
What my requirments:
- VIN: 36V-60V, Max Vin: 90V
- VOUT: 65V, Max Vout: 100V,
- Synchronous Boost, Current mode control