Hello,
we have a flyback design using LM3481. Vin is 5.3V. We measure 5V at the VCC pin buffered with 1uF. As we are blow 6V the internal BIAS circuit should be disabled and the Vin voltage forwarded to the VCC pin. The VCC pin voltage should driving the DR pin8 and Vgate. In series to the gate we are using a 1Ohm resistor. However, VCC with 5V seems to be different from the DR Voltage which rather equals Vin.
Current sense resistor is 220mOhm setting around 700mA peak limit which we do not hit. From time to time we do see a switching waveform of the DR pin and the VDS of the FET which seems to be like tow levels. The DR Pin does not switch from 0V to VCC but has a step in between. Please see the attached scope plot.
What is the explanation for this?
We can repeat this with several boards.
Orange: VCC
Yello: VGate
Green : VDS
many thanks
Lutz