Hi,
I am looking into the PMID_GOOD operation during boost mode OCP. When I(SYS_OCP_Q4) reached, would PMID_GOOD latched at low following the stop of boost mode, or back to high after boost mode stopped?
Best Regards,
Peiheng.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am looking into the PMID_GOOD operation during boost mode OCP. When I(SYS_OCP_Q4) reached, would PMID_GOOD latched at low following the stop of boost mode, or back to high after boost mode stopped?
Best Regards,
Peiheng.
Peiheng,
Referring to 8.3.8.4 PMID Voltage Indicator (PMID_GOOD), Once PMID voltage is out of this range, PMID_GOOD goes LOW to disconnect the accessory device from PMID. During boost mode, all the conditions to exit boost mode will drive PMID_GOOD from HIGH to LOW, including boost mode disable in register, ACOV, TS fault, battery depleted (VBAT_DPL), BATFET over-current, (ISYS_OCP_Q4), etc.
Thanks,
Ning.