Hi
I have LM34936 and the inductor and R5,D1 is getting pretty warm, temp close to 60C, can you explain if this is normal or do I have to increase the pad under these components.
Is this normal or not
The input voltage 24V
Input current 1.5A
Output voltage 12V
Output current 4A
Thank you