Hi team,
My customer have new project.
They are applied to a monitoring system that uses a battery as a power source. In extreme conditions, the battery voltage may be lower than 1.5V. The high efficiency of TPS63802 seems to be suitable for their application, but the data sheet show that the input voltage must be greater than 1.8 V can be started. At this time, if the product is restarted after being powered off, there seems to be a risk that it will not start normally? In terms of use or circuit design, is there any suggestion to avoid this restriction?
Thanks and best regards,
Jamie