This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: ucc28780

Part Number: UCC28780


Ulrich

I am still having an issue: The start up depletion FET is not turning off in time. Then it will burn up the resistor or the zeners!

So we put fatty parts. Like 1K/.5W  instead of 121 Ohms. And robust 20V zeners. Recall BSS FET has  Rds(ON)=700 Ohm, ours 4.5 Ohms so we can initially be equivalent with 1k in series.

Still, I burnt up the resistor.

But I do see VDD ramping up , going down & repeating the cycle as I ramp up VBULK..only to the extent I could ...because the resistor smoked out.

#1 SWS & HVG are not shorted. Which would keep the FET ON.

#2 We have 909k with 2200pF..measurable...perhaps not related with startup.

#3 C3909  SOT89 pkg is robust ..so it is intact.

# 4: Considered possibility that HVG pin is not soldered..but doubt although we will check early Monday morning.

If I understood the mechanism correctly, with VBULK,  VSW ramps up to 17.5V & then starts towards steady-state value. The FET will remain ON due to the GS resistor( maintaining Vgs=0, ON) until HVG is pulled by the controller to be below  source by Vth of CPC3909.. I do not read this explained exactly as I write here but seems this ought to be the mechanism for protecting the parts. That FET must turn  OFF in less than 25 usec, right?

So the explanation I have is HVG pin not connected.

Any other thoughts?

-Any help will be highly appreciated.

-robin