Other Parts Discussed in Thread: LM61460
I want to use the TPS56637 (or possibly the LM61460) to generate 5V at up to a few amps (4A to 6A, I'm not sure yet). I'll be plugging the 5V line it generates into a circuit that may or may not already be powered (separately) by a different source at around 5V (maybe a tad higher or lower). [It is known that this other (USB) power source will not sink current, i.e. it will not try to actively pull down a voltage higher than its own regulated voltage, so from its perspective this is ok.]
Is this situation also ok for the TPS56637 (or the LM61460)? Or, do I need to protect such switching regulators against possible reverse current using, e.g., a LM74700 and an appropriately sized MOSFET?