Hi all
My customer has this specification: Vin= 15V -26V, Vout=24V, Iout=13A.
The LM5122 should fit here and using a boost (instead of a buck-boost) is preferred due to the lower number of FETs.
What happens if Vin > Vout, in this case Vin=26V ?
They wouldn't mind the output voltage going to 26V.
Best regards
Ueli