Hello,
Using the LM1117 as an example I want to hear your opinion on this?
I am making sure I meet the LM1117 requirement of 0.3 - 22 ohm ESR on my 22 uF output capacitor and I do the layout as suggested with the shortest and widest possible traces. But then my +3.3V rail goes on to the loads and these loads have e.g. a bunch of 100nF 0402 ceramic decoupling caps each having an ESR as low as 30 mohm.
In the case of relatively low static currents (<200mA) and small transients I have historically kind of forgot or even ignored about this ESR and capacitance contribution.
How do you reason reason about this ESR and capacitance contribution?
Regards,
/Gunnar Alm