This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61391: TPS61391 without using the current mirror

Part Number: TPS61391

Hello Support,

I want to use the TPS61391 without the current monitor, I just need a boost converter. I learned from another thread that I can leave the current mirror pins (AVCC, CAP, APD, MONIN, MON1, MON2) open when the current mirror is not used. Judging from the Block Diagram the could also be the case for ISHORT. Can you confirm that?

But when I do a design in the Webench Power Designer, I have the option to disable the current mirror, and the schematics has still components on all the current mirror pins. Are these component actually needed? I'm confused, who is right, the Webench or the forums?

Regards