This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LM62435-Q1: Convertion of input 24VDC to stable 5V @3A

Prodigy 250 points

Replies: 1

Views: 46

Part Number: LM62435-Q1

Hi,

I am planning to use "LM62435-Q1" for converting 24VDC to 5V, 3A.

5V is supplied to external components (Load cell) using a connector, in industrial environment.

5V@3A supply should be stable as this is the important requirement for our customer.

Is "LM62435-Q1" part is suitable for the above purpose? If not please suggest me which part goes well with the requirement.

Thanks,

Dinesh KS

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.