Hi
LM5179 this device is used for battery learning machine products. The current application will over the max rating.
For HV, it will be 150V and for LV, it will be 120V. The peak voltage might up to 180V.
We would like to understand the risk if the input/output voltage are over the spec. Can the risk be manageable? There might have some risk on VIN, SW, CSACSB and BRKGBRSK pins, and we might have the solutions for VIN, CSACSB and BRKGBRSK pins. How about SW pin? Can SW pin be managed if input/output voltages are over the spec. ?
or is there any other device recommendation for the application? Thanks.