Other Parts Discussed in Thread: LP8863-Q1
Hello Team, following request from customer:
I understand that display mode will set all LEDs with the same brightness and cluster mode will be able to set brightness independently for all 4 outputs. I have questions about LED control for LP8860.
- I can see brightness registers, but I can’t see any control register for enable/disable out1~out4. Is there no this kind of register?
- In display mode, is it able to enable/disable only one output of out1~out4? Or say all 4 outputs must be on/off the same time?
- In cluster mode, the adaptive mode for boost voltage output is disabled. Why is the adaptive mode disabled for cluster mode ? Any difficulty for applying adaptive mode for cluster mode?
- Do you have similar LED driver with similar adaptive mode and independent control strings on/off? ( we have three strings)
The reasons that I’m asking above questions:
- we have difficulty for our stuck_on diagnostic since we have 11 leds in series ( using out2~out4 in cluster mode), to cover worst case forward voltage, we need set boost voltage to higher side. Hence that, it’ll cause out2~4 is higher than the voltage level it’s supposed to be and make difficulty to diagnose them.
- we don’t care if all of them out1~out4 brightness set to the same since we only enable one string each time, we don’t mix color. If in display mode, each channel can enable/disable independently, then we can use display mode. If all selected outx must on/off at the same time, then display mode is not good for our application.
- We want to improve our led stuck_on, stuck_off, short and open diagnostic
Thanks
Josef