This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2664: Is there a dual output device providing ±5V?

Part Number: LM2664
Other Parts Discussed in Thread: TLV2711, TPS65130

Hello. I wish to power the TLV2711 low power Op Amp, supplying ±5V.

When testing with my prototype, I used the USB 5V and LM2664M6X to create -5V.

Now, I have to use a LiPo 3.7V with 200mAh battery instead.

Considering the power consumption and the IC size, is there a dual output device providing ±5V to power the TLV2711 from TI?

The input will be the LiPo 3.7V. Thanks for your kind help.