Other Parts Discussed in Thread: , BQSTUDIO
Hello,
By the document SLUAA42, it seems there are no features changed in the HW and the FW of BQ28Z610 can be ported to the BQ28Z610-R1: it is good because the BQ28Z610 will be replaced by the -R1 version, and they could be mixed in the batches of our battery boards, so I will avoid to have to different setup for the same product. Is this correct?
In the last Technical Reference of BQ28Z610, SLUUA65D, I find some commands and settings which are not available with the FW v0.20, while they are surely available in the FW v1.01 for the revised HW version BQ28Z610-R1 (whose Technical Reference is SLUUC81). Then, I am wondering if I can use the FW BQ28Z610-R1 v1.01_Build 29 to update the FW of BQ28Z610 v0.17_Build 22 and v0.20_Build 25. The features of protection against unbalance it's interesting (and useful, too).
Thanks a lot
Maurizio