This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62823: About rated voltage of SW pin

Part Number: TPS62823

Dear teams,

When I checked the voltage of the SW pin, it was over rated.

The voltage of the SW pin exceeds Vin+0.3V, and the time exceeding Vin is longer than 10ns, so the relaxation condition cannot be applied.

Are there any problems?

Condition : input voltage =5V, output voltage=3.3V, output current=0.1A

Best regards,