This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62740: power saving

Part Number: TPS62740

Hi 

Currently tuning low power saving
U5 TPS62740DSS PIN5 (VOUT 3.3V) connect to low power MCU,
Other loads are connected to PIN6 (LOAD), PIN4 (CTRL) is controlled by MCU, set to LOW, no power supply
Powered by BATT_SYS-1 DC 3.8V to U5 (TPS62740DSS), MCU enters Shutdown mode, about, this is a series of ammeter on the power supply terminal of U5 measured 130uA
Theoretically, MCU enters shutdown only 1uA, but now it is 130uA

Do you have any suggestions to improve the current consumption of TPS62740DSS at light load?